Question about Using HyperRam and HyperFlash

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Question about Using HyperRam and HyperFlash

Jump to solution
3,545 Views
ChekhovMark
Contributor II

Hi, I have some problems developing an I.MX 1052 application. I need more GPIOs, and flash speed is critical. so I'm thinking about using HyperRam and HyperFlash instead of QSPI Flash and SDRAM. Is it posssible to mount both HyperRam and HyperFlash simultaneously on one flexSPI instance, and XIP boot from HyperFlash? If I do so, will the access speed drop when accessing RAM and FLASH together?

Thanks.

Labels (3)
0 Kudos
Reply
1 Solution
3,361 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Chekhov Mark,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)  Is it possible to mount both HyperRam and HyperFlash simultaneously on one FlexSPI instance, and XIP boot from HyperFlash?
-- No, I'm afraid not.
For the MIMXRT1052, it's capable of working with the HyperRam and HyperFlash simultaneously, as it has the FlexSPI A and FlexSPI B.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
3,361 Views
jeremyzhou
NXP Employee
NXP Employee

Hi Chekhov Mark,

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1)  Is it possible to mount both HyperRam and HyperFlash simultaneously on one FlexSPI instance, and XIP boot from HyperFlash?
-- No, I'm afraid not.
For the MIMXRT1052, it's capable of working with the HyperRam and HyperFlash simultaneously, as it has the FlexSPI A and FlexSPI B.

pastedImage_1.png

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply