Program fails when accessing DTCM

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Program fails when accessing DTCM

Jump to solution
2,160 Views
CktDesigner
Contributor IV

I'm using the MIMXRT1060-EVKB evaluation board, so the CPU being used is MIMXRT1062DVL6B.

So I expect the on chip SRAM to be 1 Mbyte or 0x100000

I'm also using MCUXpresso to develop code...

I have a program that instantiates a large uint8_t (byte) array.

The program works when using the "default" IDE settings (Execute out of SDRAM).

The program has a loop that marches through this large array.

However, my target application wants to execute out of ITCM and use DTCM for data.

I modified the MCU settings (C/C++ Build -> MCU settings) to have the following TCM regions:

SRAM_ITC   Start at: 0x2000        Size: 0x3E000

SRAM_DTC Start at: 0x20000000 Size: 0x80000

SRAM_OC   Start at: 0x20200000 Size: 0x40000

SRAM_ITC_RESERVE Start at: 0x0  Size: 0x2000

So the sum of all of the SRAM sections is 0x100000

I also changed C/C++ Build -> Settings -> MCU Linker -> Managed Linker Settings

     Checked the "Link application to RAM"

     Heap in SRAM_OC Region

     Stack in SRAM_DTC Region (Location Start)

     and added an extra-linker script input section:

     *(.bss*)        SRAM_DTC

When I build, everything links as expected.

When I run the TCM version, things start as expected, but the code "hangs" (no exceptions invoked).

Further debugging shows that when the DTCM accesses cross over the boundary between 0x2001feff to 0x20020800  (crossing over the 0x2001ffff to 0x20020000 boundary, accesses to DTCM fail.

Is there something else I need to do to "configure" the memory arrangement (beyond the setup in MCU settings)?

I also tried changing the "extra" linker statement to point all .bss to SDRAM (  *(.bss*)  BOARD_SDRAM ) and the program ran as expected... So the execution from ITCM seems to work.     But accessing beyond 0x2001ffff seems to cause a problem.

Suggestions?

Thanks!

Labels (1)
0 Kudos
Reply
1 Solution
2,094 Views
CktDesigner
Contributor IV

I now realize that filling out the memory configuration in MCU settings doesn't create the code to actually configure the I/D TCM.     So modifications need to be made in "start_mimxrt1062.c" to configure the SRAM banks...    (And since the system is running from ITCM from boot, the bank loaded via the "default" fuse settings needs to stay the same...)

View solution in original post

0 Kudos
Reply
4 Replies
2,134 Views
CktDesigner
Contributor IV

It appears that changing MCU settings (in particular the memory configuration) doesn't update board.c

This is where the MPU (memory protection unit) gets set up.    It looks like the DTCM region is limited here to 128K bytes...

Is there a configuration area that should be modified to change the contents of board.c?   Or is it expected that board.c be edited manually?

 

0 Kudos
Reply
2,131 Views
CktDesigner
Contributor IV

I modified the MPU setup in "board.c" to reflect the sizes of ITCM, DTCM, and OC_SRAM.  

It didn't seem to make a difference.  I still get a bus fault when accessing DTCM beyond the 128K boundary.

Suggestions?

0 Kudos
Reply
2,095 Views
CktDesigner
Contributor IV

I now realize that filling out the memory configuration in MCU settings doesn't create the code to actually configure the I/D TCM.     So modifications need to be made in "start_mimxrt1062.c" to configure the SRAM banks...    (And since the system is running from ITCM from boot, the bank loaded via the "default" fuse settings needs to stay the same...)

0 Kudos
Reply
2,137 Views
CktDesigner
Contributor IV

An update...

Further debugging shows that a fault was taken (but the code then loops)...

Here is the Memory Configuration in MCUXpresso:

MCUXpresso Memory ConfigurationMCUXpresso Memory Configuration

Here is the Linker configuration:

MCUXpresso Linker ConfigurationMCUXpresso Linker Configuration

Here is the Bus Fault report:   

Bus Fault when accessing 0x20020800Bus Fault when accessing 0x20020800

It can be seen that the fault occurs when attempting to access 0x20020800.    This address should be within the range of DTCM...     It almost appears that the system thinks that DTCM is only 128K bytes in length.

My assumption is that I only need to edit these tables (Memory configuration, linker configuration, etc.) and then do a project "clean" and a project "build".    Are there other steps that I missed?

Did I configure something improperly?

Thanks...

0 Kudos
Reply