Problem with debugging RT1062 on Ulink2

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem with debugging RT1062 on Ulink2

5,869 Views
NVazquez
Contributor IV

I am using RT1062 with custom made board. I cannot debug,

 

This is some of the console data,

Opening flash driver MIMXRT1060_SFDP_QSPI.cfx
Sending VECTRESET to run flash driver
Flash variant 'JEDEC_SFDP_Device' detected (16MB = 256*64K at 0x60000000)
Closing flash driver MIMXRT1060_SFDP_QSPI.cfx
Connected: was_reset=false. was_stopped=true
Awaiting telnet connection to port 3330 ...
GDB nonstop mode enabled
Opening flash driver MIMXRT1060_SFDP_QSPI.cfx (already resident)
Sending VECTRESET to run flash driver
Flash variant 'JEDEC_SFDP_Device' detected (16MB = 256*64K at 0x60000000)
Writing 13652 bytes to address 0x60002000 in Flash
Sectors written: 0, unchanged: 1, total: 1
Erased/Wrote sector 0-0 with 13652 bytes in 349msec
Closing flash driver MIMXRT1060_SFDP_QSPI.cfx
Flash Write Done
Flash Program Summary: 13652 bytes in 0.35 seconds (38.20 KB/sec)
Starting execution using system reset and halt target
Stopped (Was Reset) [Reset from Unknown]

 

 

Not sure if it is because I need to set nothing at the default Flash Driver.

Nhule_0-1634769143884.png

 

0 Kudos
Reply
6 Replies

5,854 Views
NVazquez
Contributor IV

I looked up the user guide, section 10.1(Starting a debug session) page number 78, the program stops at main() at xxx.c. But when I try to debug the program stops at Thread #11

 

Nhule_0-1634834910758.png

 

 

Not sure why I am getting stuck in Thread.

0 Kudos
Reply

5,848 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @NVazquez ,

   Thanks for your effort.

   Please let me know your used QSPI detail chip partnumber.

   Please download this SDK code to test your QSPI flash at first in the RAM:

SDK_2_10_1_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\flexspi\nor\polling_transfer

Test it, whether you can finish the external flash erase, read and program operation at first.

kerryzhou_0-1634871412194.png

 

 

Please also check your RT boot mode, whether it is the internal boot mode?  BOOT_MODE[1:0]=10.

 

Any test result, just kindly let me know.

Best Regards,

kerry

 

 

0 Kudos
Reply

5,838 Views
NVazquez
Contributor IV

The Qspi I am using is 25Q128JV.

When I tried to debug after selecting the "link application to RAM" option I was able to debug and I am transmitting something(some dots and not the correct data).

But I can't program when "Link application to RAM" is selected.

 

This is what I get.

Connected: was_reset=false. was_stopped=true
( 70) License Check Complete
File 'SerialCommProject.axf' load failure: Ef(11). No flash configured.
(100) Target Connection Failed
Unable to perform operation!
Command failed with exit code 1

 

I also had to change the size of the Flash in order to debug the code in main(), this is what I have set, I don't know if it's correct.

 

Nhule_0-1634927507075.png

 

 

What should be the boot mode set to? where can I check it?

 

I tried using MCUboot utility I was able to read and erase the flash. I can also see  in console,

 

Loading 'SerialCommProject.axf' ELF 0x60000000 len 0x4C6C
Opening flash driver MIMXRT1060_SFDP_QSPI.cfx (already resident)
Sending VECTRESET to run flash driver
Flash variant 'JEDEC_SFDP_Device' detected (16MB = 256*64K at 0x60000000)
Writing 19564 bytes to address 0x60000000 in Flash
1 of 1 ( 0) Writing sectors 0-0 at 0x60000000 with 19564 bytes
( 0) at 60000000: 0 bytes - 0/19564
(100) at 60000000: 65536 bytes - 65536/19564
Sectors written: 0, unchanged: 1, total: 1
Erased/Wrote sector 0-0 with 19564 bytes in 35msec
Closing flash driver MIMXRT1060_SFDP_QSPI.cfx
(100) Finished writing Flash successfully.
Flash Write Done
Loaded 0x4C6C bytes in 454ms (about 43kB/s)
Reset target (system)
Starting execution using system reset

0 Kudos
Reply

5,816 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @NVazquez ,

1. Do you mean you are using :W25Q128JV

This chip is the 3.3V chip:

https://datasheet.lcsc.com/szlcsc/Winbond-Elec-W25Q128JVFIQ_C111478.pdf

So, in your RT1062, do you power on it with 3.3V?

2. About the :

SDK_2_10_1_EVK-MIMXRT1060\boards\evkmimxrt1060\driver_examples\flexspi\nor\polling_transfer

running in the internal RAM, you need to modify the LUT at first.

const uint32_t customLUT[CUSTOM_LUT_LENGTH] = {

Modify :

/* Erase Sector */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0xD7, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),

to:

/* Erase Sector */
[4 * NOR_CMD_LUT_SEQ_IDX_ERASESECTOR] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x20, kFLEXSPI_Command_RADDR_SDR, kFLEXSPI_1PAD, 0x18),

 

Modify:

/* Enable Quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x01, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),

to 

/* Enable Quad mode */
[4 * NOR_CMD_LUT_SEQ_IDX_WRITESTATUSREG] =
FLEXSPI_LUT_SEQ(kFLEXSPI_Command_SDR, kFLEXSPI_1PAD, 0x31, kFLEXSPI_Command_WRITE_SDR, kFLEXSPI_1PAD, 0x04),

Modify  QE bit position:

#define FLASH_QUAD_ENABLE 0x40

to 

#define FLASH_QUAD_ENABLE 0x02

 

Then test it again, and also give me your test printf result. I need to check it.

 

3.  MCUboot utility test result is OK.

4. Please use the JLINK as the debugger, then I think you also can use the RT-UFL, you can refer to this post: 

https://community.nxp.com/t5/i-MX-RT-Knowledge-Base/RT600-MCUXpresso-JLINK-debug-QSPI-flash/ta-p/134...

As I know, the RT-UFL can support your QSPI directly.

 

Any updated information, please kindly let me know.

Best Regards,

Kerry

 

0 Kudos
Reply

5,855 Views
NVazquez
Contributor IV

I tried using J-link debugger, I am getting same result.

I confirmed the board I am using has QSPI chip, so "MIMXRT1060_SFDP_QSPI.cfx" is set correct.

This is what I get when I try to debug in the debug console,


Program stopped.
0x0020ed48 in ?? ()

Program received signal SIGINT, Interrupt.
0x0021a5c8 in ?? ()
Note: automatically using hardware breakpoints for read-only addresses.

0 Kudos
Reply

5,865 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi @NVazquez ,

  Please note, MIMXRT1060_SFDP_QSPI.cfx is used for the CMSIS DAP debugger, eg, the NXP official RT1062 board is MIMXRT1060-EVK, this on board debugger is CMSIS DAP, so your mentioned .cfx is used for the CMSIS Debugger.

  As I know, different debugger using the different the flash driver file, so our ULINK2 should calls your ULINK2 driver related flash driver.

  So, do you have any other debugger? I suggest you use the JLINK or CMSIS DAP, as this is the normal used debugger for the RT chip.  The NXP LPC-LINK2, MCU-LINK also support it.

 Please also check your customer board, whether you are using the QSPI chip which is the same as teh MIMXRT1060-EVK board, or other flash chip.

 

Wish it helps you!

Best Regards,

kerry

0 Kudos
Reply