Problem generation file .AXF

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Problem generation file .AXF

ソリューションへジャンプ
2,972件の閲覧回数
rubensjunior
Contributor IV

Hi friends!

I am developing a project with MIMXRT1052 and had a problem generating the .axf file. The code error is "Error 1". Has anyone had this kind of error? Please, I need your help.

pastedImage_1.png

Have a great day!

Rubens Júnior

ラベル(1)
1 解決策
2,898件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rubens, 

Could you please share more information about the problem that you are facing? For example:

  • Which version of MCUXpresso IDE are you using?
  • Are you trying to compile a project from the SDK? If so, which version of the SDK are you using?

Also, please share the whole output of the console, not just the screenshot of the error. This way we can have a better idea of what is causing this problem.

Regards,

Victor 

元の投稿で解決策を見る

2 返答(返信)
2,899件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rubens, 

Could you please share more information about the problem that you are facing? For example:

  • Which version of MCUXpresso IDE are you using?
  • Are you trying to compile a project from the SDK? If so, which version of the SDK are you using?

Also, please share the whole output of the console, not just the screenshot of the error. This way we can have a better idea of what is causing this problem.

Regards,

Victor 

2,898件の閲覧回数
rubensjunior
Contributor IV

victorjimenez‌,

Thank very much for your return. Today I fixed my project. My problem was with a file library, that contained a build error.

Have a great day!

Rubens Júnior.