Problem generation file .AXF

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Problem generation file .AXF

Jump to solution
2,998 Views
rubensjunior
Contributor IV

Hi friends!

I am developing a project with MIMXRT1052 and had a problem generating the .axf file. The code error is "Error 1". Has anyone had this kind of error? Please, I need your help.

pastedImage_1.png

Have a great day!

Rubens Júnior

Labels (1)
1 Solution
2,924 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rubens, 

Could you please share more information about the problem that you are facing? For example:

  • Which version of MCUXpresso IDE are you using?
  • Are you trying to compile a project from the SDK? If so, which version of the SDK are you using?

Also, please share the whole output of the console, not just the screenshot of the error. This way we can have a better idea of what is causing this problem.

Regards,

Victor 

View solution in original post

2 Replies
2,925 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Rubens, 

Could you please share more information about the problem that you are facing? For example:

  • Which version of MCUXpresso IDE are you using?
  • Are you trying to compile a project from the SDK? If so, which version of the SDK are you using?

Also, please share the whole output of the console, not just the screenshot of the error. This way we can have a better idea of what is causing this problem.

Regards,

Victor 

2,924 Views
rubensjunior
Contributor IV

victorjimenez‌,

Thank very much for your return. Today I fixed my project. My problem was with a file library, that contained a build error.

Have a great day!

Rubens Júnior.