Possible misplaced #endif in wifi middleware...

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Possible misplaced #endif in wifi middleware...

Jump to solution
641 Views
EdSutter
Senior Contributor II

I'm working with IMXRT1170EVKB and SDK_25_03_00 and stumbled on this.

Referring to function wifi_core_task() in middleware/wifi_nxp/wifidriver/wifi.c...

At line 1914 the code is...

#if defined(RW610)
        (void)wifi_imu_lock();
#else
        /* Protect the SDIO from other parallel activities */
        (void)wifi_sdio_lock();

        (void)wlan_process_int_status(mlan_adap);
#endif

#if defined(RW610)
        wifi_imu_unlock();
#else
        wifi_sdio_unlock();
#endif

 I admit that I am still learning this driver, but it sure seems like the top #endif is mistakenly commenting out the call to wlan_process_int_status if RW610 is defined.  Note that if RW610 is defined, then the code is simply...

        (void)wifi_imu_lock();
        wifi_imu_unlock();

which seems a bit suspicious.

0 Kudos
Reply
1 Solution
589 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Thank you for confirming this is not affecting. I still will notify the corresponding team.

 

Regards,

Daniel.

View solution in original post

3 Replies
623 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Thank you for your post.

By any chance, did you find any problem with this implementation?

 

Regards,

Daniel.

0 Kudos
Reply
610 Views
EdSutter
Senior Contributor II
I did not (my configuration does not have the RW610 defined); this is strictly an observation.
0 Kudos
Reply
590 Views
DanielRuvalcaba
NXP TechSupport
NXP TechSupport

Hi,

 

Thank you for confirming this is not affecting. I still will notify the corresponding team.

 

Regards,

Daniel.