I'm working with IMXRT1170EVKB and SDK_25_03_00 and stumbled on this.
Referring to function wifi_core_task() in middleware/wifi_nxp/wifidriver/wifi.c...
At line 1914 the code is...
#if defined(RW610)
(void)wifi_imu_lock();
#else
/* Protect the SDIO from other parallel activities */
(void)wifi_sdio_lock();
(void)wlan_process_int_status(mlan_adap);
#endif
#if defined(RW610)
wifi_imu_unlock();
#else
wifi_sdio_unlock();
#endif
I admit that I am still learning this driver, but it sure seems like the top #endif is mistakenly commenting out the call to wlan_process_int_status if RW610 is defined. Note that if RW610 is defined, then the code is simply...
(void)wifi_imu_lock();
wifi_imu_unlock();
which seems a bit suspicious.