Multiple application firmware

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Multiple application firmware

Jump to solution
1,841 Views
LoneWalker
Contributor I

Hi,

I am working on a solution which allow the firmware update without effecting current mode of operation.

Couple of questions that I have are:

Can ROM bootloader support multiple images e.g. one at address 0x0X and other at address 0x0Y?

Also does it have the facility to boot from a particular address based on some sort flags?

Thanks.

Labels (1)
0 Kudos
Reply
1 Solution
1,836 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can the ROM bootloader support multiple images e.g. one at address 0x0X and the other at address 0x0Y?
-- No, I'm afraid not.
2) Also does it have the facility to boot from a particular address based on some sort flags?
-- No.
Regarding your solution, I'd highly recommend you to refer to the application note to make it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,837 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Can the ROM bootloader support multiple images e.g. one at address 0x0X and the other at address 0x0Y?
-- No, I'm afraid not.
2) Also does it have the facility to boot from a particular address based on some sort flags?
-- No.
Regarding your solution, I'd highly recommend you to refer to the application note to make it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply