Maximum ADC Sample Rate

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Maximum ADC Sample Rate

1,746 次查看
scottc385
Contributor I

We are evaluating the i.MX RT 1024 for an application that requires sampling the 12-bit ADC @ 5 mega samples per second and deliver the data to memory using the EDMA. 

What is the maximum ADC sample rate of the i.MX RT 1024?

Can the EDAM be used to deliver the samples to RAM?

Thanks

标签 (1)
0 项奖励
回复
1 回复

1,739 次查看
jay_heng
NXP Employee
NXP Employee

The ADC in i.MXRT10xx and i.MXRTxxx supports 12-bit resolution, 1MS/s sampling rate.

The ADC in i.MXRT11xx supports 12-bit resolution, 4.2MS/s sampling rate.

For i.MXRT1024, EDMA can be used to deliver data

0 项奖励
回复