Max Clock Frequency of HyperRAM memory for RT1172

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Max Clock Frequency of HyperRAM memory for RT1172

跳至解决方案
1,428 次查看
LuisC
Contributor II

Hello,

 

On table 10-48 of the reference manual, I see that the max clock frequency for serial RAM is dependent on the chip. However, in other documentation I see that the max clock frequency for the FlexSPI peripheral is 166 MHz.

We are planning to use a HyperRAM chip that has a max clock frequency of 250 MHz. Will this clock speed by obtainable through FlexSPI, does the 166 MHz boundary only apply to Flash?

 

0 项奖励
回复
1 解答
1,400 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @LuisC ,

No, this restriction apply to all the device interface with FlexSPI. 250M is impossible.

 

Regards,

Jing

在原帖中查看解决方案

1 回复
1,401 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @LuisC ,

No, this restriction apply to all the device interface with FlexSPI. 250M is impossible.

 

Regards,

Jing