Max Clock Frequency of HyperRAM memory for RT1172

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Max Clock Frequency of HyperRAM memory for RT1172

ソリューションへジャンプ
1,425件の閲覧回数
LuisC
Contributor II

Hello,

 

On table 10-48 of the reference manual, I see that the max clock frequency for serial RAM is dependent on the chip. However, in other documentation I see that the max clock frequency for the FlexSPI peripheral is 166 MHz.

We are planning to use a HyperRAM chip that has a max clock frequency of 250 MHz. Will this clock speed by obtainable through FlexSPI, does the 166 MHz boundary only apply to Flash?

 

0 件の賞賛
返信
1 解決策
1,397件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @LuisC ,

No, this restriction apply to all the device interface with FlexSPI. 250M is impossible.

 

Regards,

Jing

元の投稿で解決策を見る

1 返信
1,398件の閲覧回数
jingpan
NXP TechSupport
NXP TechSupport

Hi @LuisC ,

No, this restriction apply to all the device interface with FlexSPI. 250M is impossible.

 

Regards,

Jing