MIMXRT1170 FlexSPI2 (boot device) was not accessible on Cypress(Spansion) Hyper Flash

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

MIMXRT1170 FlexSPI2 (boot device) was not accessible on Cypress(Spansion) Hyper Flash

跳至解决方案
1,167 次查看
kitsohn
Contributor I

From my MIMXRT1172 proto board design, it consist of FlexSPI2 as boot device and external SDRAM on SEMC_B1 bus ports.

But it can't access hyper flash region (0x60000000) by JTAG_ICE debugger (Lauterbach), also can't boot operation...T T;

Pls check or review how to access FlexSPI2 device memory. (BOOT CFG = 1010 0000 0000)

kitsohn_0-1660790455535.png

kitsohn_1-1660790499030.png

kitsohn_2-1660790665006.png

kitsohn_3-1660791099055.png

 

Anyone else success to boot on FlexSPI2 Hyperflash ?

Thanks,

 

0 项奖励
回复
1 解答
1,164 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In the RT1170/1160, the FlexSPI2's port has 8 data bits, so it's not necessary to use the Combination Mode to connect an Octal Flash, further FlexSPI2 doesn't support this mode.

jeremyzhou_0-1660794794505.png

 


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,165 次查看
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
In the RT1170/1160, the FlexSPI2's port has 8 data bits, so it's not necessary to use the Combination Mode to connect an Octal Flash, further FlexSPI2 doesn't support this mode.

jeremyzhou_0-1660794794505.png

 


-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 项奖励
回复