MIMXRT1170-EVK LPUARTs

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1170-EVK LPUARTs

Jump to solution
1,279 Views
andreas90
Contributor I

As far as I can tell from the schematic of the MIMXRT1170-EVK board, the only UART available for external access is LPUART1, either via J11 USB port or directly via the J31/J32 connectors. However, I've seen other people in these forums mention e.g. LPUART4 being accessible by the CM4 (https://community.nxp.com/t5/i-MX-RT-Crossover-MCUs/RT1170-EVK-how-enable-PRINTF-for-use-on-secondar...).

So to clarify, on the MIMXRT1170-EVK board, which LPUARTs can I access from which core, and which of these are actually accessible from outside?

0 Kudos
Reply
1 Solution
1,235 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @andreas90,

All LPUART modules are accessible to both cores.

As for which are accessible externally with the use of the Arduino Connector, that would be:

  • LPUART12:
    • GPIO_LPSR_06: TXD
    • GPIO_LPSR_07: RXD
  • LPUART11:
    • GPIO_LPSR_04: TXD
    • GPIO_LPSR_05: RXD
  • LPUART8:
    • GPIO_AD_02: TXD
    • GPIO_AD_03: RXD
  • LPUART7:
    • GPIO_AD_00: TXD
    • GPIO_AD_01: RXD
  • LPUART5:
    • GPIO_AD_28: TXD
    • GPIO_AD_29: RXD
  • LPUART3:
    • GPIO_AD_30: TXD
    • GPIO_AD_31: RXD
  • LPUART2:
    • GPIO_DISP_B2_10: TXD
    • GPIO_DISP_B2_11: RXD

Hope this helps!

BR,
Edwin

View solution in original post

0 Kudos
Reply
4 Replies
102 Views
RahulRaj
Contributor I

For LPUART1 J31.2 TX, J32.2 Rx and J38.9 GND so like that all pins details of each UART and is parallel it will work or not like i want to use console and UART at same time.

  • LPUART12:
    • GPIO_LPSR_06: TXD
    • GPIO_LPSR_07: RXD
  • LPUART11:
    • GPIO_LPSR_04: TXD
    • GPIO_LPSR_05: RXD
  • LPUART8:
    • GPIO_AD_02: TXD
    • GPIO_AD_03: RXD
  • LPUART7:
    • GPIO_AD_00: TXD
    • GPIO_AD_01: RXD
  • LPUART5:
    • GPIO_AD_28: TXD
    • GPIO_AD_29: RXD
  • LPUART3:
    • GPIO_AD_30: TXD
    • GPIO_AD_31: RXD
  • LPUART2:
    • GPIO_DISP_B2_10: TXD
    • GPIO_DISP_B2_11: RXD

Explain for each one.

0 Kudos
Reply
1,236 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @andreas90,

All LPUART modules are accessible to both cores.

As for which are accessible externally with the use of the Arduino Connector, that would be:

  • LPUART12:
    • GPIO_LPSR_06: TXD
    • GPIO_LPSR_07: RXD
  • LPUART11:
    • GPIO_LPSR_04: TXD
    • GPIO_LPSR_05: RXD
  • LPUART8:
    • GPIO_AD_02: TXD
    • GPIO_AD_03: RXD
  • LPUART7:
    • GPIO_AD_00: TXD
    • GPIO_AD_01: RXD
  • LPUART5:
    • GPIO_AD_28: TXD
    • GPIO_AD_29: RXD
  • LPUART3:
    • GPIO_AD_30: TXD
    • GPIO_AD_31: RXD
  • LPUART2:
    • GPIO_DISP_B2_10: TXD
    • GPIO_DISP_B2_11: RXD

Hope this helps!

BR,
Edwin

0 Kudos
Reply
166 Views
RahulRaj
Contributor I
For LPUART1 J31.2 TX, J32.2 Rx and J38.9 GND so like that all pins details of each UART and is parallel it will work or not like i want to use console and UART at same time.
0 Kudos
Reply
1,225 Views
andreas90
Contributor I

Thank you so much, that helps a lot!

0 Kudos
Reply