MIMXRT1064-EVK sensor device initialize failed

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1064-EVK sensor device initialize failed

2,204 Views
jtsai1
Contributor I

Hi 

There are two problems I have:

1.When I connect the board, The board cannot be found in "Board and Device selection page" of MCUExpresso IDE.

2.The console shows : "Sensor device initialize failed!" and "Please check the sensor chip U32".

 How to fix this problem? 

d9ccf435-b6cd-419d-a5d1-8199adce7a41.png

 

0 Kudos
Reply
2 Replies

792 Views
sateesh12
Contributor I

Well it is an MIMXRT1060-EVKB with changes done to the DIP switch SW4 to boot from QFlash, after that I am getting the error. It is connected to an Ubuntu 24.02 via Minicom.

 

Any hint please.

 

sateesh12_0-1776521960955.png

 

0 Kudos
Reply

2,199 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
Before sharing some advice, I was wondering if you can describe the testing environment, such as board, demo, IDE, etc.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply