MIMXRT1020-EVK rev A3 Schematics

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

MIMXRT1020-EVK rev A3 Schematics

ソリューションへジャンプ
7,113件の閲覧回数
amczarny
Contributor I

Hi, I have a dev board MIMXRT 1020-EVK rev A3 but I can not find a schematics for that revision. The https://www.nxp.com/webapp/Download?colCode=MIMXRT1020-EVK-Design-Files has rev B1 which has different jumpers setup (j25, j26 etc) and debugger chip. Can you please provide me with schematics for rev A3

タグ(2)
0 件の賞賛
返信
1 解決策
7,087件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just sent you the file via private message. 

Regards,
Victor 

元の投稿で解決策を見る

8 返答(返信)
6,142件の閲覧回数
mcampani72
Contributor I

Here are the schematics.

Regards

 

0 件の賞賛
返信
6,617件の閲覧回数
bretts
Contributor I

I have a Rev A3 board that I also need the schematics for, could you please provide them?

 

Thanks,

 

Brett Swimley

0 件の賞賛
返信
7,081件の閲覧回数
amczarny
Contributor I

Thanks, highly appriciated

0 件の賞賛
返信
7,088件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just sent you the file via private message. 

Regards,
Victor 

6,161件の閲覧回数
EB_A
Contributor I

I've the same issue I'm not able to find correct information on schematics and jumper present in the rev 3 board..

May you provide schematics ?

Emilio

0 件の賞賛
返信
6,449件の閲覧回数
bikenomad
Contributor IV

I need this schematic too.

0 件の賞賛
返信
6,684件の閲覧回数
andong
Contributor I

I have RevA3 board too, i need the schematics of the same , Can i please get it?

0 件の賞賛
返信
6,735件の閲覧回数
vrajesh
Contributor I

I have RevA3 board, i need the schematics of the same , Can i please get it.

0 件の賞賛
返信