MIMXRT1020-EVK rev A3 Schematics

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

MIMXRT1020-EVK rev A3 Schematics

Jump to solution
3,183 Views
amczarny
Contributor I

Hi, I have a dev board MIMXRT 1020-EVK rev A3 but I can not find a schematics for that revision. The https://www.nxp.com/webapp/Download?colCode=MIMXRT1020-EVK-Design-Files has rev B1 which has different jumpers setup (j25, j26 etc) and debugger chip. Can you please provide me with schematics for rev A3

0 Kudos
Reply
1 Solution
3,157 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just sent you the file via private message. 

Regards,
Victor 

View solution in original post

8 Replies
2,215 Views
mcampani72
Contributor I

Here are the schematics.

Regards

 

0 Kudos
Reply
2,690 Views
bretts
Contributor I

I have a Rev A3 board that I also need the schematics for, could you please provide them?

 

Thanks,

 

Brett Swimley

0 Kudos
Reply
3,154 Views
amczarny
Contributor I

Thanks, highly appriciated

0 Kudos
Reply
3,158 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello, 

I just sent you the file via private message. 

Regards,
Victor 

2,234 Views
EB_A
Contributor I

I've the same issue I'm not able to find correct information on schematics and jumper present in the rev 3 board..

May you provide schematics ?

Emilio

0 Kudos
Reply
2,522 Views
bikenomad
Contributor IV

I need this schematic too.

0 Kudos
Reply
2,757 Views
andong
Contributor I

I have RevA3 board too, i need the schematics of the same , Can i please get it?

0 Kudos
Reply
2,808 Views
vrajesh
Contributor I

I have RevA3 board, i need the schematics of the same , Can i please get it.

0 Kudos
Reply