LVGL version in SDK is lag behind

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

LVGL version in SDK is lag behind

ソリューションへジャンプ
1,572件の閲覧回数
BlackTurbo
Contributor III

I'm planing to use LVGL for our project on RT1062, but found that the LVGL version (v7.4.0) is very lag behind in the latest SDK (2.9.3, 2021.4.9), the latest LVGL is v7.11.0. Will it be updated in further SDK? What should I do if I want to use the latest version v7.11.0 on RT1062?

Thanks

0 件の賞賛
返信
1 解決策
1,566件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Will it be updated in further SDK?
-- Yes, of course.
2) What should I do if I want to use the latest version v7.11.0 on RT1062?
-- Definitely, it's available to port the v7.11.0 to RT1062, please follow the porting guide to do it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,567件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Will it be updated in further SDK?
-- Yes, of course.
2) What should I do if I want to use the latest version v7.11.0 on RT1062?
-- Definitely, it's available to port the v7.11.0 to RT1062, please follow the porting guide to do it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信