LVGL version in SDK is lag behind

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

LVGL version in SDK is lag behind

Jump to solution
1,126 Views
BlackTurbo
Contributor III

I'm planing to use LVGL for our project on RT1062, but found that the LVGL version (v7.4.0) is very lag behind in the latest SDK (2.9.3, 2021.4.9), the latest LVGL is v7.11.0. Will it be updated in further SDK? What should I do if I want to use the latest version v7.11.0 on RT1062?

Thanks

0 Kudos
Reply
1 Solution
1,120 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Will it be updated in further SDK?
-- Yes, of course.
2) What should I do if I want to use the latest version v7.11.0 on RT1062?
-- Definitely, it's available to port the v7.11.0 to RT1062, please follow the porting guide to do it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

View solution in original post

0 Kudos
Reply
1 Reply
1,121 Views
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Will it be updated in further SDK?
-- Yes, of course.
2) What should I do if I want to use the latest version v7.11.0 on RT1062?
-- Definitely, it's available to port the v7.11.0 to RT1062, please follow the porting guide to do it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 Kudos
Reply