Is it possible to use a different DMA Transfer configuration for every ADC-ETC trigger source?

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Is it possible to use a different DMA Transfer configuration for every ADC-ETC trigger source?

ソリューションへジャンプ
1,571件の閲覧回数
imxrtuser
Senior Contributor I

Hello,

for every trigger of the ADC-ETC it is possible to enable DMA

pastedImage_5.png

DMA_CTRL register of ADC-ETC peripheral:

pastedImage_6.png

but Table 3-3. DMA MUX Mapping of RT1020 Reference Manual shows only one DMA Request signal for ADC_ETC

pastedImage_4.png

Is it possible to use a different DMA Transfer configuration for every ADC-ETC trigger source?

Kind regards,

Stefan

タグ(4)
0 件の賞賛
返信
1 解決策
1,511件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan Mitterhauser

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to use a different DMA Transfer configuration for every ADC-ETC trigger source?
-- No, I'm afraid it's impossible.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

0 件の賞賛
返信
1 返信
1,512件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi Stefan Mitterhauser

Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1) Is it possible to use a different DMA Transfer configuration for every ADC-ETC trigger source?
-- No, I'm afraid it's impossible.

Have a great day,
TIC

 

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

0 件の賞賛
返信