Inline encryption engine(IEE) for External flash memory in IMXRT1170

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

Inline encryption engine(IEE) for External flash memory in IMXRT1170

跳至解决方案
2,645 次查看
Nagaveni
Contributor II

Hi, 

I am using IMXRT1170 Evk ,

  1. can I use IEE(Inline encryption engine) for both encryption and decryption to   read and write to the external flash memory ?
  2. please find below image  and can you tell us what is difference between 8.1.2 section from security RM manual and 7.10 section from IMXRT1170RM manual ?

  

Nagaveni_0-1678529927799.png

 

Nagaveni_1-1678529987132.png

Thanks in advance

 

 

0 项奖励
回复
1 解答
2,575 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you for your patience!
The IEE features on the SRM don't take the system limitations of RT1170. So IEE on RT1170 can only decrypt FlexSPI Nor memory.

Best regards,
Omar

在原帖中查看解决方案

0 项奖励
回复
3 回复数
2,603 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Hello
I hope you are well.

IEE on flexspi is only capable of decryption, however, let me confirm if it is also possible to encrypt flexspi through IEE.

Best regards,
Omar

0 项奖励
回复
2,594 次查看
Nagaveni
Contributor II

Thank you for the response,

Please confirm ASAP, Regarding IEE encryption for Flash memory

0 项奖励
回复
2,576 次查看
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Thank you for your patience!
The IEE features on the SRM don't take the system limitations of RT1170. So IEE on RT1170 can only decrypt FlexSPI Nor memory.

Best regards,
Omar

0 项奖励
回复