IMXRT1024 Suitable UART Method

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

IMXRT1024 Suitable UART Method

ソリューションへジャンプ
5,871件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi all,

 

I am between usage UART_WriteByte and UART_TransferSendNonBlocking. Which one is correct? I want just minimum delay. I know that UART_TransferSendNonBlocking is non-polling method and I will use it with interrupts.

But I see that there is a normal interrupt example in SDK with UART_WriteByte. Can I ensure same performance when I use UART_WriteByte with interrupt method ? Will they be same if I do like that ?

Will it be a polling approach, When I use only UART_WriteByte ?

Will it be a non-polling approach, When I use UART_WriteByte with interrupts?

 

Thanks and Regards.

 

0 件の賞賛
返信
1 解決策
5,783件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
The depth of Transmit and Receive buffers are 4-datawords, just like the below figure shows.

jeremyzhou_0-1630896679857.png

 


Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

元の投稿で解決策を見る

10 返答(返信)
5,840件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
1-) How can I get the received byte count that comes to my FIFO.
-- Please check the RXCOUNT bits.

jeremyzhou_0-1630293250115.png


2-) What is the best way to use polling, interrupt or eDMA?
-- In my opinion, you can choose the interrupt or eDMA way.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,827件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi again Dear @jeremyzhou ,

 

I've tried that watching that registers in debug mode. But, issue comes like that; I am setting FIFO size with related registers 256 word (despite it is stated as read-only, I am a little bit confused in here. In this question LPUART_FIFO , @danielchen stated it can be configurable) and I am expecting RXCOUNT represents 256 word but it is always being 4 word and decreasing like 3-2-1-0 at the end of transmission.

 

Why we are not able to watch TX/RXCOUNT as actual FIFO size?

 

Thanks and Regards.

0 件の賞賛
返信
5,815件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
1) Why we are not able to watch TX/RXCOUNT as actual FIFO size?
-- The FIFO buffer depth is fixed, in another, is not configurable.

Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,806件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou ,

 

Then, what is the actual size of FIFO Buffer Depth ?

 

Thanks and Regards.

0 件の賞賛
返信
5,794件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou ,

 

Could you please reply me? This question was for approval. Will I not be able to set and use my FIFO size as 256 word? Will it be just 4 word as defaultly stated in MIMXRT1024_features.h below?

 

/* @brief Capacity (number of entries) of the transmit/receive FIFO (or zero if no FIFO is available). */
#define FSL_FEATURE_LPUART_FIFO_SIZEn(x) (4)

 

Thanks and Regards.

 
タグ(1)
0 件の賞賛
返信
5,784件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
The depth of Transmit and Receive buffers are 4-datawords, just like the below figure shows.

jeremyzhou_0-1630896679857.png

 


Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,774件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou,

 

Will I not be able to set these depth as 256-word? Is there no possibility?

Lukas_Frank_0-1631000964183.png

Thanks and Regards.

0 件の賞賛
返信
5,748件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thanks for your reply.
1) Will I not be able to set these depth as 256-word? Is there no possibility?
-- No, you can't.
Hope this is clear.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,861件の閲覧回数
jeremyzhou
NXP Employee
NXP Employee

Hi,
Thank you for your interest in NXP Semiconductor products and for the opportunity to serve you.
To be prudent, I was wondering if you can describe what kind of data the UART will transmit, then I'll share the advice with you to do it.
Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------

5,850件の閲覧回数
Lukas_Frank
Senior Contributor I

Hi Dear @jeremyzhou,

 

I will transmit and receive datagram packages between length 70 to 250 words.

I wonder about two topics as follows:

 

1-) How can I get received byte count that comes to my FIFO.

2-) What is the best way to use polling, interrupt or eDMA? 

 

Thanks and Regards.

0 件の賞賛
返信