How to put a big array in OCRAM?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to put a big array in OCRAM?

Jump to solution
844 Views
simmania
Contributor IV

Hi,
I'm usingMCUXpresso with  MIMXRT1010-EVK hardware.

In my program I need a big array. The linker tries to put this in the SRAM_DTC (which I assume is the DTCM). But there is not enough room. While the SRAM_OC (which I assume is the OCRAM) is completely empty.
So, how to instruct the linker to put my big array in SRAM_OC?

Is there some tutorial about this kind of memory management stuff?

0 Kudos
Reply
1 Solution
839 Views
simmania
Contributor IV

Ok, I found it out.
So here is how I did it, in case other people may want to know:

In the Properties of the project, under C/C++ Build -> MCU settings, I could see that the OCRAM section has the alias 'RAM3'. (here you also can change the sizes of the RAM sections)

Then in the code you can do:

#include <cr_section_macros.h>

__DATA(RAM3) uint16_t buffer[BUFSIZE];

 

View solution in original post

0 Kudos
Reply
1 Reply
840 Views
simmania
Contributor IV

Ok, I found it out.
So here is how I did it, in case other people may want to know:

In the Properties of the project, under C/C++ Build -> MCU settings, I could see that the OCRAM section has the alias 'RAM3'. (here you also can change the sizes of the RAM sections)

Then in the code you can do:

#include <cr_section_macros.h>

__DATA(RAM3) uint16_t buffer[BUFSIZE];

 

0 Kudos
Reply