How to enable memory mapping of the Flexspi controller?

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to enable memory mapping of the Flexspi controller?

803 次查看
thomas82
Contributor I

Hi,
I'm working with an i.MXRT1064 microcontroller and since I have to communicate with a QSPI Flash I'm using the FlexSPI controller.
I used as a starting point the example "flexspi_nor_polling_transfer" of the SDK and the i.MX RT1064 EVK board.
The example works correctly and when I write/erase the QSPI Flash I get confirmation from Keil's 'windows' tool as the memory mapped mode is active.

The problem is that I can't use memory mapped mode on a custom board that uses the same microcontroller.
If I send a GetInfo command to the QSPI Flash it replies correctly, but it is as if the memory mapped mode was not active.
Do I have to configure it somehow?
The code written mirrors the example of the SDK mentioned above.

Greetings,
Thomas

0 项奖励
回复
0 回复数