Hello,
We want to use USB of MIMXRT1062 as device mode only.
We would like to use OTG1_PWR, OTG1_OC and OTG1_ID as GPIO because we do not use the OTG function.
The questions are
Q1. To disable OTG and enable device mode only, can I just set the CM register in 42.7.33 USB Device Mode (USB_nUSBMODE) to Device Controller?
Q2. Are there any precautions when using
USB_OTG1_PWR (GPIO_AD_B0_02, GPIO_AD_B1_01)
USB_OTG1_OC (GPIO_AD_B0_03, GPIO_AD_B1_03)
USB_OTG1_ID (GPIO_AD_B0_01, GPIO_AD_B1_02)
as GPIO?
解決済! 解決策の投稿を見る。
Hi,
No, I think nothing need to aware.
Regards,
jing