How to configure headphone mic in IMXRT1050 evk

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure headphone mic in IMXRT1050 evk

1,318 Views
yogesh_modi
Contributor II

Hello,

I'm trying to configure the Headphone Mic for audio input instead of On-board Mic for Tesnsorflow_kws example,

I'm already using OMTP headphones and I tried

 wm8960Config.leftInputSource = kWM8960_InputDifferentialMicInput3;

but it is not working, So please let me know how can I configure the headphone mic

 

Thanks & Regards

Yogesh

0 Kudos
Reply
2 Replies

1,296 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi yogesh_modi,

  It turns out you modify the wrong place.

  Please note, image.png

image.png

phone mic is circuited to the Left input in the codec, so you need to write the wm8960config like this:

wm8960_config_t wm8960Config = {
.i2cConfig = {.codecI2CInstance = BOARD_CODEC_I2C_INSTANCE, .codecI2CSourceClock = BOARD_CODEC_I2C_CLOCK_FREQ},
.route = kWM8960_RoutePlaybackandRecord,
.rightInputSource = kWM8960_InputDifferentialMicInput2,
.leftInputSource = kWM8960_InputDifferentialMicInput3,
.playSource = kWM8960_PlaySourceDAC,
.slaveAddress = WM8960_I2C_ADDR,
.bus = kWM8960_BusI2S,
.format = {.mclk_HZ = 6144000U, .sampleRate = kWM8960_AudioSampleRate16KHz, .bitWidth = kWM8960_AudioBitWidth16bit},
.master_slave = false,
};

You need to add the leftinput source as the phone mic.

I have tested it on my side, it works now.

Wish it helps you!

If you still have questions about it, please kindly let me know!

Best Regards,

Kerry

-------------------------------------------------------------------------------

Note:

- If this post answers your question, please click the "Mark Correct" button. Thank you!

 

- We are following threads for 7 weeks after the last post, later replies are ignored

Please open a new thread and refer to the closed one, if you have a related question at a later point in time.

-----------------------------------------------------------------------------

0 Kudos
Reply

1,305 Views
kerryzhou
NXP TechSupport
NXP TechSupport

Hi yogesh_modi,

   Except for the  codec input channel modification, I still didn't find any other place to modify it, today I test the Sai playback code with a headphone mic, also not a success, tomorrow, I will check with some of our experts.

  After I get the valuable feedback, I will let you know.

Please keep patient, thanks.

 

Best Regards,

Kerry

0 Kudos
Reply