How to configure External SAI MCLK source in Peripherals Config Tool

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

How to configure External SAI MCLK source in Peripherals Config Tool

跳至解决方案
2,222 次查看
gh78731
Contributor III

I need to connect an I2S ADC to SAI1 on an iMX RT1050. I am currently using a hacked iMX RT1050 EVK as the hardware. The I2S ADC will be the master clock source for all three I2S clocks.  The Peripherals config Tool allows me to set the RX_SYNC clock and the RX_BCLK to an external source, but I can't find any setting to set the SAI1_MCLK to an external clock source.

How and where do I do this?

Is it sufficient to set the SAI1_MCLK pin to input? Or is there more to it than that?

Thanks, --- Graham

0 项奖励
回复
1 解答
2,208 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

From my understanding to your description you are using the SAI module as a slave. If this is the case, then when using SAI as a slave, there usually is no need to select an MCLK, because
bit clock and frame sync are generated externally. 

Best Regards,

Sabina

 

在原帖中查看解决方案

1 回复
2,209 次查看
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

From my understanding to your description you are using the SAI module as a slave. If this is the case, then when using SAI as a slave, there usually is no need to select an MCLK, because
bit clock and frame sync are generated externally. 

Best Regards,

Sabina