How to configure External SAI MCLK source in Peripherals Config Tool

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

How to configure External SAI MCLK source in Peripherals Config Tool

Jump to solution
2,145 Views
gh78731
Contributor III

I need to connect an I2S ADC to SAI1 on an iMX RT1050. I am currently using a hacked iMX RT1050 EVK as the hardware. The I2S ADC will be the master clock source for all three I2S clocks.  The Peripherals config Tool allows me to set the RX_SYNC clock and the RX_BCLK to an external source, but I can't find any setting to set the SAI1_MCLK to an external clock source.

How and where do I do this?

Is it sufficient to set the SAI1_MCLK pin to input? Or is there more to it than that?

Thanks, --- Graham

0 Kudos
Reply
1 Solution
2,131 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

From my understanding to your description you are using the SAI module as a slave. If this is the case, then when using SAI as a slave, there usually is no need to select an MCLK, because
bit clock and frame sync are generated externally. 

Best Regards,

Sabina

 

View solution in original post

1 Reply
2,132 Views
Sabina_Bruce
NXP Employee
NXP Employee

Hello ,

Hope you are doing well.

From my understanding to your description you are using the SAI module as a slave. If this is the case, then when using SAI as a slave, there usually is no need to select an MCLK, because
bit clock and frame sync are generated externally. 

Best Regards,

Sabina