How to add program protection function to RT1060 and RT1064

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

How to add program protection function to RT1060 and RT1064

2,692 次查看
lw3
Contributor I

How to add program protection function to RT1060 and RT1064

Prohibit reading programs through SWD or serial or USB methods

Can encryption function be enabled

Can the flash run normally when switched to another MCU

How to Prevent Copying Flash and Replacing with Other RT1060 MCUs from Running Properly

0 项奖励
回复
8 回复数

2,667 次查看
lw3
Contributor I

After adding read protection to the jlink swd interface

Can we use the swd port of jlink to download new programs again in the future

0 项奖励
回复

2,660 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @lw3 ,

Yes, please refer to AN12419.

 

Regards,

0 项奖励
回复

2,633 次查看
lw3
Contributor I
Can you give me the download connection for AN12419
0 项奖励
回复

2,624 次查看
jingpan
NXP TechSupport
NXP TechSupport
0 项奖励
回复

2,573 次查看
lw3
Contributor I
I'll study how to use it
0 项奖励
回复

2,573 次查看
lw3
Contributor I
Thank you
0 项奖励
回复

2,677 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi @lw3 ,

To prevent unauthorized read from SWD/JTAG, you should enable SJTAG.

To prevent copy code, you should use BEE and encrypt the code in flash.

 

Regards,

Jing

0 项奖励
回复