FreeRTOS LPSPI Example Project

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FreeRTOS LPSPI Example Project

3,311 Views
nbgatgi
Contributor IV

I recently downloaded the SDK v2.6 for the iMX RT1064 eval board (evkmimxrt1064).  The documentation file for FreeRTOS (Getting Started with MCUXpresso SDK and FreeRTOS OS.pdf - Attached) mentions in Table 1. List of Examples that there is an example project for "freertos_lpspi":

 

pastedImage_1.png

 

However, when I try to "Import SDK example(s)..." from MCUXpresso, this example is not listed under "rtos_examples" or "driver_examples>lpspi".

 

pastedImage_3.png

 

Any idea if the "freertos_lpspi" example actually exists, and if so where can I find it?

1 Reply

2,989 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Nick,

I answered directly on your other community post.


Have a great day,
TIC

-------------------------------------------------------------------------------
Note:
- If this post answers your question, please click the "Mark Correct" button. Thank you!

- We are following threads for 7 weeks after the last post, later replies are ignored
Please open a new thread and refer to the closed one, if you have a related question at a later point in time.
-------------------------------------------------------------------------------