FlexIO Question: Simultaneous Peripheral Use?

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FlexIO Question: Simultaneous Peripheral Use?

Jump to solution
1,822 Views
lsrbigfoot
Contributor IV

Can a single FlexIO peripheral be used to perform 2 transactions at once?

For example, FlexIO2 pins (shifters, and timers) were allocated for two (2) separate SPI ports connected to different devices. Can FlexIO2 be configured to initiate SPI transactions on both ports simultaneously? Or must each FlexIO2 transaction happen one port at a time?

Tags (2)
0 Kudos
Reply
1 Solution
1,791 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @lsrbigfoot,

The FlexIO peripheral is not capable of preforming two transactions at once. You can definitely connect more than one device to the same SPI pins from the FlexIO, but it would have to be according to the SPI specification, where SCLK, MOSI and MISO are in a shared bus, and the CS lines are connected directly to each device.

BR,
Edwin.

View solution in original post

0 Kudos
Reply
1 Reply
1,792 Views
EdwinHz
NXP TechSupport
NXP TechSupport

Hi @lsrbigfoot,

The FlexIO peripheral is not capable of preforming two transactions at once. You can definitely connect more than one device to the same SPI pins from the FlexIO, but it would have to be according to the SPI specification, where SCLK, MOSI and MISO are in a shared bus, and the CS lines are connected directly to each device.

BR,
Edwin.

0 Kudos
Reply