Dear Sir,
We are attempting to make custom boards for one of our display application, only with required interfaces from IMXRT1050-EVKB using hyper-flash and MCU. But we would like to have a JTAG port at both the development version and production version. Planned to remove the OpenSDA adaptor function in this custom board, in this case, I have the following queries:
1. I assume bootloader code part of hyper-flash, how do I flash bootloader into it? Is it via JTAG? For any procedure document please share to flash bootloader into Hyperflash.
2. Share the bootloader image link to download.
3. How to flash application binary/hex (built via MCU expresso IDE or others IDE) into target MCU using the JTAG interface?
4. Is it a mandate to have MCUexpresso IDE to flash the application binary/hex file? Suggest the flash loader through which I should flash binary/hex file without IDE using JTAG.
5. Is it possible to flash application binary and bootloader to together?
6. Which is the best practise (Flash bootloader separate and application file separate or flash them together), please advice?
Before making a custom board we need to decide above software development lifecycle tools & procedures. Please clarify.
Development system of our display with EVAL board is attached for reference