FLEXSPI Used for Code & Data

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

FLEXSPI Used for Code & Data

2,553 Views
sagar_prajapati
Contributor II

Hello all,

I am using IMXRT1064 evaluation board. I am using XIP mode. I want to store some configuration data to internal QSPI flash which is connected to FLEXSPI2. So this kind of configuration is possible or not?

And if yes and then please provide documentation or some example project files.

Labels (1)
0 Kudos
Reply
2 Replies

2,429 Views
davidrozenski
Contributor I

Hi,

You need to put all QSPI functions (lik erase, write etc) in RAM and disable, enable IRQ when calling.

regards

0 Kudos
Reply

2,429 Views
fangfang
NXP TechSupport
NXP TechSupport

Hello,

Yes, It is possible.

Unfortunately, There is not the related document for it.

Best regards

Tic

0 Kudos
Reply