Hi
Can i.MXRT support two displays simultaneously?
Does embedded Wizard support the development of dual display applications on an i.MXRT ?
Many thanks
Dani
Hi Dani,
The RT doesn't support two displays simultaneously.
Regards,
Victor
Hi Victor,
In the reference manual (i.MX RT1170 Processor Reference Manual, Rev. 1, 05/2021 page 2990) I find a block diagram that seems to suggest that dual display is possible. There are two arrows pointing at 
Display 1. "To Display"
Display 2. "LCD Display"
Does this suggest that dual display with i.MX RT1170 is possible?
Man thanks
Dani
Hi Dani,
You are right on this, I apologize for the confusion on my end. Theoretically, the combination of the MIPI-DSI interface and Parallel RGB interface is possible, but it was not tested.
Regards,
Victor 
Hello Victor,
Does NXP plan to perform any verification tests for this or to confirm this option?
Thanks
Ido
Hello Ido,
Unfortunately, there aren't any plans to test this.
Regards,
Victor