Dual Display with iMXRT using embedded Wizard

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Dual Display with iMXRT using embedded Wizard

8,151件の閲覧回数
danielgull
Contributor IV

Hi

Can i.MXRT support two displays simultaneously?

Does embedded Wizard support the development of dual display applications on an i.MXRT ?

Many thanks

Dani

タグ(1)
0 件の賞賛
返信
6 返答(返信)

8,136件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Dani, 

The RT doesn't support two displays simultaneously. 

Regards,
Victor

0 件の賞賛
返信

8,080件の閲覧回数
danielgull
Contributor IV
 
0 件の賞賛
返信

8,079件の閲覧回数
danielgull
Contributor IV

Hi Victor,

In the reference manual (i.MX RT1170 Processor Reference Manual, Rev. 1, 05/2021 page 2990) I find a block diagram that seems to suggest that dual display is possible. There are two arrows pointing at 
Display 1. "To Display"

Display 2. "LCD Display"

Does this suggest that dual display with i.MX RT1170 is possible?

Man thanks

Dani

 

0 件の賞賛
返信

8,058件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Dani, 

You are right on this, I apologize for the confusion on my end. Theoretically, the combination of the MIPI-DSI interface and Parallel RGB interface is possible, but it was not tested. 

Regards,
Victor 

 

0 件の賞賛
返信

7,990件の閲覧回数
idolevi
Contributor IV

Hello Victor,

Does NXP plan to perform any verification tests for this or to confirm this option?

Thanks
Ido

0 件の賞賛
返信

7,983件の閲覧回数
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ido,

Unfortunately, there aren't any plans to test this. 

Regards,
Victor 

0 件の賞賛
返信