Dual Display with iMXRT using embedded Wizard

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Dual Display with iMXRT using embedded Wizard

5,855 次查看
danielgull
Contributor IV

Hi

Can i.MXRT support two displays simultaneously?

Does embedded Wizard support the development of dual display applications on an i.MXRT ?

Many thanks

Dani

标记 (1)
0 项奖励
回复
6 回复数

5,841 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Dani, 

The RT doesn't support two displays simultaneously. 

Regards,
Victor

0 项奖励
回复

5,785 次查看
danielgull
Contributor IV
 
0 项奖励
回复

5,784 次查看
danielgull
Contributor IV

Hi Victor,

In the reference manual (i.MX RT1170 Processor Reference Manual, Rev. 1, 05/2021 page 2990) I find a block diagram that seems to suggest that dual display is possible. There are two arrows pointing at 
Display 1. "To Display"

Display 2. "LCD Display"

Does this suggest that dual display with i.MX RT1170 is possible?

Man thanks

Dani

 

0 项奖励
回复

5,763 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Dani, 

You are right on this, I apologize for the confusion on my end. Theoretically, the combination of the MIPI-DSI interface and Parallel RGB interface is possible, but it was not tested. 

Regards,
Victor 

 

0 项奖励
回复

5,695 次查看
idolevi
Contributor IV

Hello Victor,

Does NXP plan to perform any verification tests for this or to confirm this option?

Thanks
Ido

0 项奖励
回复

5,688 次查看
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ido,

Unfortunately, there aren't any plans to test this. 

Regards,
Victor 

0 项奖励
回复