Dual Display with iMXRT using embedded Wizard

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

Dual Display with iMXRT using embedded Wizard

8,105 Views
danielgull
Contributor IV

Hi

Can i.MXRT support two displays simultaneously?

Does embedded Wizard support the development of dual display applications on an i.MXRT ?

Many thanks

Dani

Tags (1)
0 Kudos
Reply
6 Replies

8,090 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Dani, 

The RT doesn't support two displays simultaneously. 

Regards,
Victor

0 Kudos
Reply

8,034 Views
danielgull
Contributor IV
 
0 Kudos
Reply

8,033 Views
danielgull
Contributor IV

Hi Victor,

In the reference manual (i.MX RT1170 Processor Reference Manual, Rev. 1, 05/2021 page 2990) I find a block diagram that seems to suggest that dual display is possible. There are two arrows pointing at 
Display 1. "To Display"

Display 2. "LCD Display"

Does this suggest that dual display with i.MX RT1170 is possible?

Man thanks

Dani

 

0 Kudos
Reply

8,012 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hi Dani, 

You are right on this, I apologize for the confusion on my end. Theoretically, the combination of the MIPI-DSI interface and Parallel RGB interface is possible, but it was not tested. 

Regards,
Victor 

 

0 Kudos
Reply

7,944 Views
idolevi
Contributor IV

Hello Victor,

Does NXP plan to perform any verification tests for this or to confirm this option?

Thanks
Ido

0 Kudos
Reply

7,937 Views
victorjimenez
NXP TechSupport
NXP TechSupport

Hello Ido,

Unfortunately, there aren't any plans to test this. 

Regards,
Victor 

0 Kudos
Reply