Debug Error on OCRAM

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Debug Error on OCRAM

1,178件の閲覧回数
SpeedyGonzalesss
Contributor III

Hello,

I am using i.MX RT1176 and MCU xPRESSO IDE.I am running the code in OCRAM. This structure works with the bootloader. But I have problems when I want to debug the app code without the bootloader.

SpeedyGonzalesss_0-1739251462887.png

How can i fix this?

Memory settings:

SpeedyGonzalesss_1-1739251512916.png

**Link app to ram actived.

Best Regards,

Fatih

0 件の賞賛
返信
2 返答(返信)

1,156件の閲覧回数
SpeedyGonzalesss
Contributor III

In the ResetHandler(), I encounter this problem after entering the while loop written for the copying process from flash to SRAM.

SpeedyGonzalesss_0-1739262254780.png

 

0 件の賞賛
返信

1,102件の閲覧回数
Habib_MS
NXP Employee
NXP Employee

@SpeedyGonzalesss,
Sorry for my misunderstanding but I cannot see the issue in this image, can you provide me more information about this issue?

Also, the SDK (version 24.12) provides an example called "flexram_ram_allocate_cm7" where is used an OCRAM.
BR
Habib

0 件の賞賛
返信