Connection to VBUS in IMXRT1176

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Connection to VBUS in IMXRT1176

642件の閲覧回数
priyanka09
Contributor I

Hi Team

I am using one module on USB2 interface of IMXRT1176. Module is powered up using external 3.3V and VDD_USB_3P3 and VDD_USB_1V8 pins of IMXRT are powered using 3.3V and 1.8V respectively. 

Do I need to connect USB2_VBUS also to 5V or it can be left floating/any other recommendation if supply current to peripheral device is not required from VBUS?

As per the below architecture, I got that USB PHYs are powered using VDD_USB_3P3 and VDD_USB_1V8 and VBUS is not required. 

priyanka09_0-1705041606405.png

 

 

0 件の賞賛
返信
1 返信

591件の閲覧回数
diego_charles
NXP TechSupport
NXP TechSupport

Hi @priyanka09 

Many thanks for your patience. 

Let me provide a general reply :  If the MCU's USB2 module will act as a device, it does not need to provide voltage on VBUS. So,  in this scenario, you can let USB2_VBUS  floating .This is according to the USB 2.0 specification

diego_charles_0-1706113414942.png

Reference is USB_20.pdf from here: https://www.usb.org/document-library/usb-20-specification

If this is not help, could you let me know more about your intended USB application? Are you designing a self-powered device and VBUS will never get any power from the host anyway?

 

Best regards, 

Diego

 

0 件の賞賛
返信