Cannot enter the Debug session- MIMXRT1176DVMAA

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

Cannot enter the Debug session- MIMXRT1176DVMAA

1,107 次查看
S_Rai
Contributor I

Hello ,

 

i am working on MaaXBoard RT V3 board with MIMXRT1176DVMAA controller for an application of interface with External flash,

I have imported the out of box demo application from github 

GitHub - Avnet/MaaXBoard-RT-V3--GUI-Demo: Reference design for the MaaXBoard RT Rev.03 hardware demo...

 

when i debug the project from MCUXresso IDE i am getting the following error

Awaiting telnet connection to port 3330 ...
GDB nonstop mode enabled
FreeRTOS stack backtrace is disabled in Non-stop mode (use All-stop)
After error Nn(05). Wire ACK Wait in DAP access -
Failed to read address register in DAP - Nn(05). Wire ACK Wait in DAP access
Target error from Write Memory: Em(17). Debug port inaccessible after access at location 0x80000000
GDB stub (C:\nxp\MCUXpressoIDE_11.6.0_8187\ide\plugins\com.nxp.mcuxpresso.tools.bin.win32_11.6.0.202207121507\binaries\crt_emu_cm_redlink) terminating - GDB protocol problem: Pipe has been closed by GDB.
state - running or following reset request - re-read of state failed - rc Nn(05). Wire ACK Fault in DAP access

i have disabled the XIP_EXTERNAL_FLASH preprocessor.below is the screen shot of the preprocessor settings.

S_Rai_0-1666714712717.png

below is the screenshot of MCU memory settings

S_Rai_1-1666714807646.png

What might be the issue?

 

Regards

Sanath

 

0 项奖励
回复
2 回复数

1,070 次查看
danielchen
NXP TechSupport
NXP TechSupport

Hi

There is a similar issue about ‘Wire ACK Wait in DAP access’ discussed here

https://community.nxp.com/t5/MCUXpresso-General/Error-when-flashing-to-MIMXRT1050-EVKB-quot-Wire-ACK...

 

Regards

Daniel

0 项奖励
回复

1,088 次查看
S_Rai
Contributor I

Hi,

 

Any suggestion on above issue will be appreciated .Thank you.

Is it Project settings issue?

Regards

sanath

0 项奖励
回复