Brownout detection on i.MXRT1064 microcontroller using MCUXpresso IDE

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

Brownout detection on i.MXRT1064 microcontroller using MCUXpresso IDE

ソリューションへジャンプ
1,173件の閲覧回数
wavhal_m
Contributor II

Hello,

I'm using following code for brownout detection. I included fsl_pmu.h and fsl_pmu.c in the code. However, I observed that IRQ is not getting served. Kindly suggest the corrections in the code.

void Brownout_Init(void){
//Enable 1.1V brownout circuitry in the LDO
PMU_1P1EnableBrownout(PMU, TRUE);
 
//Set LDO output voltage to 1.1V
PMU_1P1SetRegulatorOutputVoltage(PMU, 0x10);
 
//Set LDO brownout offset voltage to 0.175V
PMU_1P1SetBrownoutOffsetVoltage(PMU, 0x7);
 
//Enable LDO output
PMU_1P1EnableOutput(PMU, TRUE);
 
//Enable 2.5V brownout circuitry in the LDO
PMU_2P5nableBrownout(PMU, TRUE);
 
//Set LDO output voltage to 2.5V
PMU_2P5SetRegulatorOutputVoltage(PMU, 0x10);
 
//Set LDO brownout offset voltage to 0.175V
PMU_2P5SetBrownoutOffsetVoltage(PMU, 0x7);
 
//Enable LDO output
PMU_2P5EnableOutput(PMU, TRUE);
 
NVIC_EnableIRQ(PMU_EVENT_IRQn);
}
 
void ANATOP_EVENT0_IRQHandler(void)
{
  const uint32_t status = PMU_GetStatusFlags(PMU);
 // uint16_t result = 0;
 
  if (status & kPMU_1P1BrownoutOnOutput)
  {
    // result = kPMU_1P1BrownoutOnOutput;
  }
 
  if (status & kPMU_2P5BrownoutOnOutput)
  {
    // result = kPMU_2P5BrownoutOnOutput;
  }
}
 
I'm having one more doubt, in the User Manual it is said that -
The following bitfields are not applicable on this device, and
those corresponding bits are Reserved:
• in PMU_REG_COREn register:
• RAMP_RATE
• REG2_TARG
• REG1_TARG
• REG0_TARG
• in PMU_MISC1n register: IRQ_DIG_BO.
• in PMU_MISC2n register:
• REG2_STEP_TIME
• REG1_STEP_TIME
• REG0_STEP_TIME
• REG2_OK
• REG2_ENABLE_BO
• REG1_ENABLE_BO
 
I found similar bitfields are also available in the register - CCM_ANALOG_MISC2n and this register is shared with PMU. So may I use CCM_ANALOG_MISC2n, instead of using PMU_MISC2n register? And its support is available in fsl_pmu.c?
0 件の賞賛
返信
1 解決策
1,132件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this post to turn on the brownout detector: Solved: Re: How to enable brownout detection - NXP Community

These fields do not apply to the device even when accessing through CCM registers since they share space.
Please refer to the driver, it uses different registers to enable and set the BO.

Best regards,
Omar

元の投稿で解決策を見る

1 返信
1,133件の閲覧回数
Omar_Anguiano
NXP TechSupport
NXP TechSupport

Please refer to this post to turn on the brownout detector: Solved: Re: How to enable brownout detection - NXP Community

These fields do not apply to the device even when accessing through CCM registers since they share space.
Please refer to the driver, it uses different registers to enable and set the BO.

Best regards,
Omar