About NOR Flash Write/Read in ASYNC mode (Non-ADMUX) at SEMC

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 
已解决

About NOR Flash Write/Read in ASYNC mode (Non-ADMUX) at SEMC

跳至解决方案
1,947 次查看
george
Senior Contributor II

Dear All,

Please tell me about Flash Write in ASYNC mode (Non-ADMUX) using SEMC.

The reference manual only gives examples for ADMUX mode, but how are the addresses assigned when using non-ADMUX mode?

pastedImage_1.png

Maybe SEMC_ADDR [8:0] is assigned to A [8:0]?

Please tell me one more thing.

What does the following note mean?

Maybe, Does this mean that there are few addresses available?

pastedImage_15.png

BR,

George

0 项奖励
回复
1 解答
1,841 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi George,

I have learnt that SEMC module implemented in i.MXRT1050 doesn't support non-ADMUX mode. So the customer need to use ADMUX or AADM mode only.

Regards,

Jing

在原帖中查看解决方案

0 项奖励
回复
1 回复
1,842 次查看
jingpan
NXP TechSupport
NXP TechSupport

Hi George,

I have learnt that SEMC module implemented in i.MXRT1050 doesn't support non-ADMUX mode. So the customer need to use ADMUX or AADM mode only.

Regards,

Jing

0 项奖励
回复