About NOR Flash Write/Read in ASYNC mode (Non-ADMUX) at SEMC

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

About NOR Flash Write/Read in ASYNC mode (Non-ADMUX) at SEMC

Jump to solution
1,188 Views
george
Senior Contributor II

Dear All,

Please tell me about Flash Write in ASYNC mode (Non-ADMUX) using SEMC.

The reference manual only gives examples for ADMUX mode, but how are the addresses assigned when using non-ADMUX mode?

pastedImage_1.png

Maybe SEMC_ADDR [8:0] is assigned to A [8:0]?

Please tell me one more thing.

What does the following note mean?

Maybe, Does this mean that there are few addresses available?

pastedImage_15.png

BR,

George

0 Kudos
Reply
1 Solution
1,082 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi George,

I have learnt that SEMC module implemented in i.MXRT1050 doesn't support non-ADMUX mode. So the customer need to use ADMUX or AADM mode only.

Regards,

Jing

View solution in original post

0 Kudos
Reply
1 Reply
1,083 Views
jingpan
NXP TechSupport
NXP TechSupport

Hi George,

I have learnt that SEMC module implemented in i.MXRT1050 doesn't support non-ADMUX mode. So the customer need to use ADMUX or AADM mode only.

Regards,

Jing

0 Kudos
Reply