yocto web server ntp

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 
17,600件の閲覧回数
niklasmolin
Senior Contributor I

Hi.

I'm pretty new with the Yocto environment.

Trying to figure out what webserver that is included in the Yocto environment (which I can include as a package and how I do that).

I also tried to include a ntp client, but couldn't figure out how to do that.

Thanks,

Niklas

ラベル(2)
0 件の賞賛
返信
1 解決策
9,934件の閲覧回数
LeonardoSandova
Specialist I

Sure Dan. niklasmolin, I am not sure if this is the package you need

http://layers.openembedded.org/layerindex/branch/master/recipes/?q=ntpdate

In the future, try to check that search engine for yocto layers/recipes. If the package you are looking for is there, just clone the repo under sources, then modify your corresponding bblayers.conf to include this new layer, then add the recipe on your local.conf.

Leo

元の投稿で解決策を見る

0 件の賞賛
返信
8 返答(返信)
9,934件の閲覧回数
niklasmolin
Senior Contributor I

I found lighthttpd as a web browser, but I decided to compile nginx and use that one instead (since I have to take that path later anyway).

I still haven't figure out the NTP client (what package or flag I need to add to my local.conf to include the ntp client)?

9,934件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Niklas,

http://www.brennan.id.au/09-Network_Time_Protocol.html this link is talking about NTP , you can take a reference, hope this can help you~~

Best Regards

Dan

0 件の賞賛
返信
9,934件の閲覧回数
niklasmolin
Senior Contributor I

Hi Dan.

Thanks for the update.

The problem I have is that I don't have the ntpdate application in my build.

That's what I'm trying to figure out how to include that when I'm building my image.

Best regards,

Niklas

0 件の賞賛
返信
9,934件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi LeonardoSandovalGonzalez , could you help this issue? I am mot familiar with Yocto. Thanks a lot .

Best Regards,

Dan

0 件の賞賛
返信
9,935件の閲覧回数
LeonardoSandova
Specialist I

Sure Dan. niklasmolin, I am not sure if this is the package you need

http://layers.openembedded.org/layerindex/branch/master/recipes/?q=ntpdate

In the future, try to check that search engine for yocto layers/recipes. If the package you are looking for is there, just clone the repo under sources, then modify your corresponding bblayers.conf to include this new layer, then add the recipe on your local.conf.

Leo

0 件の賞賛
返信
9,934件の閲覧回数
niklasmolin
Senior Contributor I

Hi Leo.

Thanks for the reply.

That search engine was really helpful to find other packages I was looking for.

I had one problem when I tried to add the meta-opie layer. Bitbake complains that I can't include 'ssh-server-openssh' in IMAGE_FEATURES.

How do I get around that if I want to include recipes from that layer?

Thanks,

Niklas

0 件の賞賛
返信
9,934件の閲覧回数
Rita_Wang
NXP TechSupport
NXP TechSupport

Hi Niklas,

You can reference i.MX6 Yocto Environment Setup , the link is https://community.freescale.com/docs/DOC-95327. There are a lot of information on Yocoto, you can search in our community.

Hope this can help you ~~

Best Regards

Dan


0 件の賞賛
返信
9,934件の閲覧回数
niklasmolin
Senior Contributor I

Hi Dan.

Thanks for your response.

When I tried to access that page I got following message:

Access to this place or content is restricted. If you think this is a mistake, please contact your administrator or the person who directed you here.


Thanks,

Niklas

0 件の賞賛
返信