yocto toolchain problem: missing headers

キャンセル
次の結果を表示 
表示  限定  | 次の代わりに検索 
もしかして: 

yocto toolchain problem: missing headers

ソリューションへジャンプ
4,115件の閲覧回数
marshall123
Contributor II

Dear Community

i meet problems installing the meta-toolchain in my computer.the system suggested that i successfully installed the toolchain

pastedImage_1.png

but when i use the toolchain it just said that the headers are not inculded

pastedImage_2.png

then i found the header directory is ignored because of "nonexistent" but thet do exist in my computer and is exactly the same name as the directory which is ignored.

pastedImage_3.png

can you help me solve the problem?

if i use the adt-installer, i will meet the same problem.

ラベル(2)
0 件の賞賛
返信
1 解決策
3,764件の閲覧回数
marshall123
Contributor II

well, I solved it by using $CC to do the compile

元の投稿で解決策を見る

0 件の賞賛
返信
4 返答(返信)
3,764件の閲覧回数
Yuri
NXP Employee
NXP Employee

Hello,

 

   Please look at the following :

https://community.nxp.com/thread/394804 

Have a great day,

Yuri

 

------------------------------------------------------------------------------

Note: If this post answers your question, please click the Correct

Answer button. Thank you!

------------------------------------------------------------------------------

0 件の賞賛
返信
3,764件の閲覧回数
marshall123
Contributor II

nope, I don't think it solved the problem, it may because the headers is not linked to the tool chain.

I want to know how to link it to the toolchain.

or every time i have to use the script to run the toolchain.and the other headers may be also missing.

0 件の賞賛
返信
3,764件の閲覧回数
Yuri
NXP Employee
NXP Employee

Please look at the following :

https://community.nxp.com/docs/DOC-173488 

Regards,

Yuri.

0 件の賞賛
返信
3,765件の閲覧回数
marshall123
Contributor II

well, I solved it by using $CC to do the compile

0 件の賞賛
返信