The ramp picture problem

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

The ramp picture problem

1,813 次查看
deshenggao
Contributor II

Dear All:

    We  use the i.MX6dual with the MIPI input function.

And we found that when we setting the MIPI as  RGB24  format.

We  will see that the test pattern RAMP picture is not smooth, you can see the green stripe.

(Please see the attach file ramp(RGB24).png),

ramp(RGB24).png

if  we changed the MIPI to YUV422 format.

You will not see the problem (Please see the attach file ramp(YUV422).png), 

ramp(YUV422).png

Which part or which  register should I check?

Thank you ! 

标签 (1)
0 项奖励
回复
2 回复数

1,743 次查看
jamesbone
NXP TechSupport
NXP TechSupport

What Camera are you using?   I think the problem it is not in the  MIPI interface, since when you change the format the image gets clear,  so  what  version it is required by your camera?

0 项奖励
回复

1,743 次查看
deshenggao
Contributor II

Hi Jamesbone:

    I do not use the camera. I use the signal generator . I also  use the ADV7480 which can  output  MIPI  signal supported  both YUV422  and RGB888 to do the test. and only  RGB888 format  have this issue,  so I guess that some

registers or place should be noticed in the i.MX6.

Please give me some advices .

Thank you!

0 项奖励
回复