yocto takes too long to compile when building SDK tools

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

yocto takes too long to compile when building SDK tools

6,027 次查看
2548903578
Contributor III

When I use yocto to build the sdk tool, I have been stuck in do_compile after using the bitbake meta-toolchain-qt5 command. It has been more than ten hours. The picture on the picture is that I started again. I want to ask is this appearance normal? Does normal compilation take so long?090232v8hxbh8oaa8b84j4.png

标签 (1)
0 项奖励
回复
10 回复数

5,587 次查看
eleven94726
Contributor I
Hi:
  I have the same problem  as you.can you tell me  how you solved it?
 
 
0 项奖励
回复

5,563 次查看
kef2
Senior Contributor V

Make sure you have enough RAM to not keep swapping to HDD, which may take forever. Use htop to check swap usage. Limiting bitbake parallel tasks to be less than CPU threads you may reduce min. RAM requirements. Keep checking swap usage, it should be 0 in the best case.

0 项奖励
回复

5,546 次查看
eleven94726
Contributor I
Thank you very much for your reply.The problem seems to be solved but my virtual machine keeps freezing.
0 项奖励
回复

5,572 次查看
2548903578
Contributor III

如果您使用的是虚拟机,我建议您将虚拟机的配置更改为更高级别,然后重试

0 项奖励
回复

6,015 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @2548903578 

This is normal

0 项奖励
回复

6,009 次查看
2548903578
Contributor III

Hi, Qmiller

   Thank you very much for your reply, how long will this process take?

0 项奖励
回复

6,006 次查看
Zhiming_Liu
NXP TechSupport
NXP TechSupport

At least 6 hours

0 项奖励
回复

5,990 次查看
2548903578
Contributor III

Hi,Qmiller

Now I have compiled more than 80 hours and still not finished. Is there a problem with this situation?微信截图_20230109082524.png

0 项奖励
回复

5,980 次查看
edwardtyrrell
Senior Contributor I

Hi @2548903578,

To build Yocto in any reasonable time you need a machine with some serious horsepower, and if you're using a VM that doesn't help.. Also the first build does all the package fetching; if your internet connection is slow the build will drag. Good news is future builds are a lot quicker once all the packages are on board. If the build is still creeping along it might just be slow internet speeds between you and the package server.

0 项奖励
回复

5,972 次查看
2548903578
Contributor III

Hi,edwardtyrrell

   Thank you for your reply, now it has been compiled, and it is indeed a problem with the virtual machine. The configuration of the virtual machine needs to be modified.

0 项奖励
回复