yocto takes too long to compile when building SDK tools

cancel
Showing results for 
Show  only  | Search instead for 
Did you mean: 

yocto takes too long to compile when building SDK tools

6,036 Views
2548903578
Contributor III

When I use yocto to build the sdk tool, I have been stuck in do_compile after using the bitbake meta-toolchain-qt5 command. It has been more than ten hours. The picture on the picture is that I started again. I want to ask is this appearance normal? Does normal compilation take so long?090232v8hxbh8oaa8b84j4.png

Labels (1)
0 Kudos
Reply
10 Replies

5,596 Views
eleven94726
Contributor I
Hi:
  I have the same problem  as you.can you tell me  how you solved it?
 
 
0 Kudos
Reply

5,572 Views
kef2
Senior Contributor V

Make sure you have enough RAM to not keep swapping to HDD, which may take forever. Use htop to check swap usage. Limiting bitbake parallel tasks to be less than CPU threads you may reduce min. RAM requirements. Keep checking swap usage, it should be 0 in the best case.

0 Kudos
Reply

5,555 Views
eleven94726
Contributor I
Thank you very much for your reply.The problem seems to be solved but my virtual machine keeps freezing.
0 Kudos
Reply

5,581 Views
2548903578
Contributor III

如果您使用的是虚拟机,我建议您将虚拟机的配置更改为更高级别,然后重试

0 Kudos
Reply

6,024 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

Hi @2548903578 

This is normal

0 Kudos
Reply

6,018 Views
2548903578
Contributor III

Hi, Qmiller

   Thank you very much for your reply, how long will this process take?

0 Kudos
Reply

6,015 Views
Zhiming_Liu
NXP TechSupport
NXP TechSupport

At least 6 hours

0 Kudos
Reply

5,999 Views
2548903578
Contributor III

Hi,Qmiller

Now I have compiled more than 80 hours and still not finished. Is there a problem with this situation?微信截图_20230109082524.png

0 Kudos
Reply

5,989 Views
edwardtyrrell
Senior Contributor I

Hi @2548903578,

To build Yocto in any reasonable time you need a machine with some serious horsepower, and if you're using a VM that doesn't help.. Also the first build does all the package fetching; if your internet connection is slow the build will drag. Good news is future builds are a lot quicker once all the packages are on board. If the build is still creeping along it might just be slow internet speeds between you and the package server.

0 Kudos
Reply

5,981 Views
2548903578
Contributor III

Hi,edwardtyrrell

   Thank you for your reply, now it has been compiled, and it is indeed a problem with the virtual machine. The configuration of the virtual machine needs to be modified.

0 Kudos
Reply