yocto project sdk question

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

yocto project sdk question

1,081 次查看
strive
Contributor I

board name:sabresd

linux:yocto project     kernel version:3.14.52

question:

After I install sdk(deployed by bitbake),there is four files in 3.14.52-1.1.1,those are:

sysroots

environment-setup-cortexa9hf-vfp-neon-poky-linux-gnueabi

site-config-cortexa9hf-vfp-neon-poky-linux-gnueabi

version-cortexa9hf-vfp-neon-poky-linux-gnueabi

Could you tell me what function  this file "site-config-cortexa9hf-vfp-neon-poky-linux-gnueabi" is?

thanks.

标签 (1)
0 项奖励
回复
1 回复

925 次查看
igorpadykov
NXP Employee
NXP Employee

Hi Tom

seems this is part of CONFIG_SITE, description can be found on

http://docs.openembedded.ru/siteinfo_class.html

Best regards
igor
-----------------------------------------------------------------------------------------------------------------------
Note: If this post answers your question, please click the Correct Answer button. Thank you!
-----------------------------------------------------------------------------------------------------------------------

0 项奖励
回复