yocto hob error

取消
显示结果 
显示  仅  | 搜索替代 
您的意思是: 

yocto hob error

5,309 次查看
心刚王
Contributor II

hi,community!

       i want to create an image for my imx6 device (use yocto hob),but i got an error as below,

      Trying to resolve runtime dependency libgl resulted in conflicting PREFERRED_PROVIDER entries being found.

The providers found were: ['/disk/workspace/imx6/yocto/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.0-hfp.bb', '/disk/workspace/imx6/yocto/sources/poky/meta/recipes-graphics/mesa/mesa_9.1.6.bb']

The PREFERRED_PROVIDER entries resulting in this conflict were: ['PREFERRED_PROVIDER_virtual/libgl = gpu-viv-bin-mx6q', 'PREFERRED_PROVIDER_virtual/mesa = mesa']

Thanks & Regards,

标记 (3)
7 回复数

3,443 次查看
durmus
Contributor IV

Hi,

The following workaround works for me, though I'm not sure if it is a proper thing to do:

Since there are 2 conflicting PREFERRED_PROVIDERs, I've just removed the one in /sources/poky/...

I've edited the line in the file mesa-gl_9.2.5.bb (your version might be different) inside the folder /fsl-release-bsp/sources/poky/meta/recipes-graphics/mesa as follows:

PROVIDES = "virtual/libgl virtual/mesa" ---->>>> PROVIDES = ""

And that's it. I'm now able to build images for i.MX6 using hob in daisy.

3,443 次查看
joëlesponde
Contributor III

Hi,

Thanks Durmus for your workaround !!

For Yocto Fido 1.8, I had to modify two files:

- sources/poky/meta/recipes-graphics/mesa/mesa.inc

- sources/poky/meta/recipes-graphics/mesa/mesa-gl_10.4.4.bb

3,443 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Unfortunately this is a known issue when using metadata from daisy on HOB so if using daisy you would need to use bitbake regularly. I'm sorry for the inconvenience.

0 项奖励
回复

3,443 次查看
gavingreenwalt
Contributor III

Just to be clear.  HOB doesn't work With daisy for i.MX6?  Is there a work around?

0 项奖励
回复

3,443 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Unfortunately that's correct, HOB does not work because of some conflicts on the Freescale BSP (it is not related to poky daisy strictly speaking). There is not a work around as of today.

3,443 次查看
dauphinalexandr
Contributor II

hi,

I'd like to know if the problem occurs only for daisy or there is the same problem for the other branchs   ?

Thank you!

0 项奖励
回复

3,443 次查看
gusarambula
NXP TechSupport
NXP TechSupport

Only in Daisy that I know of. Hob works okay with Dora. I haven't tried it with Dizzy personally but HOB will be replaced by Toaster.