hi,community!
i want to create an image for my imx6 device (use yocto hob),but i got an error as below,
Trying to resolve runtime dependency libgl resulted in conflicting PREFERRED_PROVIDER entries being found.
The providers found were: ['/disk/workspace/imx6/yocto/sources/meta-fsl-bsp-release/imx/meta-fsl-arm/recipes-graphics/gpu-viv-bin-mx6q/gpu-viv-bin-mx6q_3.10.17-1.0.0-hfp.bb', '/disk/workspace/imx6/yocto/sources/poky/meta/recipes-graphics/mesa/mesa_9.1.6.bb']
The PREFERRED_PROVIDER entries resulting in this conflict were: ['PREFERRED_PROVIDER_virtual/libgl = gpu-viv-bin-mx6q', 'PREFERRED_PROVIDER_virtual/mesa = mesa']
Thanks & Regards,
Hi,
The following workaround works for me, though I'm not sure if it is a proper thing to do:
Since there are 2 conflicting PREFERRED_PROVIDERs, I've just removed the one in /sources/poky/...
I've edited the line in the file mesa-gl_9.2.5.bb (your version might be different) inside the folder /fsl-release-bsp/sources/poky/meta/recipes-graphics/mesa as follows:
PROVIDES = "virtual/libgl virtual/mesa" ---->>>> PROVIDES = ""
And that's it. I'm now able to build images for i.MX6 using hob in daisy.
Hi,
Thanks Durmus for your workaround !!
For Yocto Fido 1.8, I had to modify two files:
- sources/poky/meta/recipes-graphics/mesa/mesa.inc
- sources/poky/meta/recipes-graphics/mesa/mesa-gl_10.4.4.bb
Unfortunately this is a known issue when using metadata from daisy on HOB so if using daisy you would need to use bitbake regularly. I'm sorry for the inconvenience.
Just to be clear. HOB doesn't work With daisy for i.MX6? Is there a work around?
hi,
I'd like to know if the problem occurs only for daisy or there is the same problem for the other branchs ?
Thank you!